Hi All.
I spent several days trying to read/write the DM365 GPIO still with any success. From the other threads I understand that there is not an "official" driver so that everyone has to develop his own (I think almost all the developers have to deal with the gpio). I tried both to use the example provided by Bernie Thompson
http://e2e.ti.com/support/embedded/f/354/p/7633/30198.aspx#30198,
and writing my own driver from the beginning. In both cases I am able to manage the GPIO from the module (for instance reading a register from the init routine), but when I try to manage the registers from the application I am not able to open the device (e.g. the command open("/dev/user_gpio", O_RDWR) fails).
Reading the thread referenced in the link above, I see the problem is common to other users. A thing which is still obscure to me regards the creation of the /dev/user_gpio. According to Juan "it appears this should be created by the driver and you should not have to type mknod". I tried:
A) do nothing: /dev/user_gpio is not created
B) mknod /dev/user_gpio c 60 0 /dev/user_gpio is created but when I open it from my application it fails.
C)
int devno = MKDEV(60,0);
in user_gpio_init_module () . Here, quite surprisingly, /dev/user_gpio is not created. chmod 666 /dev does not fix this problem.
I suppose I am missing some trivial step, any hints will be greatly appreciated.