Hi All,
I am new to Zoom development so may have missed the obvious...
I got my new Zoom 2 MDK two days back and flashed the x-loader(MLO), u-bootloader(u-boot.bin) and kernel image (zImage) on Zoom's NAND using the fastboot procedure mentioned in the "http://omappedia.org/wiki/Android_Getting_Started" wiki page. The binaries were built on my computer using the android git repository (so not very sure about their integrity). Now I am not able to talk to device via debug board (through FTDI USB-serial device) - no prompt appearing on the terminal. Also, when i plug in the USB to Zoom 2 main board, I do not see any new device in the USB device list on my computer (earlier it was appearing as Texas Instruments cafe..). The Zoom screen is showing no display and as soon as I turn ON the device, the blue led goes ON and stays ON (no red led glowing or any blinking).
I am guessing that there was some problem with the x-loader that I flashed onto the NAND. So could anyone tell me how to get control of the device so that I may flash the prebuilt images to test the device.
Thanks in advance,
Bhupinder.