This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

da830-omapL137 User Interface Push Buttons

Other Parts Discussed in Thread: PCF8574

 Greetings,

  I was wondering if anybody has come across the same problem that I.

while programing an user interface in Qt for the da830-omapl137 I need

to use the user interface push buttons as keyboard keys to generate events

that can be read from Qt.

I have tried with the gpio-keys interface but with no luck,

I also tried the pcf8574_keypad driver (which is out of main branch) with some modifications since it is ment for a matrix keypad but unfortunately

it does not work, I have manage to sense the push buttons from user space with

an example application posted in this forum :

http://e2e.ti.com/support/arm174_microprocessors/omap_applications_processors/f/42/p/29281/101800.aspx#101800

that uses the i2c driver but what really would solve the problem is a driver that can generate

keyboard events.