Other Parts Discussed in Thread: UNIFLASH
Hi Team,
am using beagle bone black and 3.12 kernel ,task is flash all image files into emmc through usb using uniflash
i configure the ip and all image files kept in one folder , when i start start flashing the ip loss and device manager usb device will disappear.so i check log file below errors so how to solve this problem please help me ...
Error log :
usb_ether
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC d0:39:72:3b:89:4e
HOST MAC de:ad:be:af:00:00
RNDIS ready
musb-hdrc: peripheral reset irq lost!
high speed config #2: 2 mA, Ethernet Gadget, using RNDIS
ERROR: The remote end did not respond in time.
at ether.c:2392/usb_eth_init()
Problem booting with BOOTP
### ERROR ### Please RESET the board ###
Regards,
Naveen