Other Parts Discussed in Thread: DM3730
Hi,
1. I'm using dvsdk_4.02.00.06, and I've connected an eMMC to SD/MMC2 of DM3730, and a sd slot to the SD/MMC1 port on my customed board.
My plan is to boot the cpu from eMMC, and I can find the MLO (copied to the FAT32 partition of the eMMC in advance)
is running after power on. But finally, it tried to load the u-boot from sd card even though no sd card is plugged at all from the beginning of powering
on. I have expected that the board boot up without sd card. It seems the code need modified, any recommendations/advice about the modification?
2. If I boot from a SD card, at the u-boot prompt, when I saveenv I get an error because there's not a nand on my board. So I do need to save env args
to SD card or eMMC, but it seems need to modify u-boot code also, any recommendations/advice about the modification?