This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IP of Remote Terminal in HTTP_Example

MCU: TM4C1294NCPDT

TI-RTOS: v2.01.00.03

NDK: v2.23.01.01

CCS: v6.0.1.0040

Hello,

    In the httpServer example (processors.wiki.ti.com/.../TI-RTOS_HTTP_Example), how do I get the IP address of the remote terminal from where the HTTP request is coming. I need to respond with different HTML content based on the PC from which the request is coming.

Thanks

Regards

Soumyajit