Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Hi everyone,
I have struggled about one month to flash u-bootais.bin into my custom omapl138 board Nor flash. My custom board have DDR2 flash and Nor flash. And i use CCS Nor writer to flash and serial flash sfh_OMAP-L138.exe , but both failed. Who have any idea please share with me .Thanks
Here is the detail:
1. Use the CCS Nor Writer to load the uboot to the Nor flash. I use the gel file OMAP-L138_LCDK.gel and confirm the system clk is 300Mhz and DDR2 clk is 150Mhz.The simulator is XD200. Then i use the CCS to open th Nor Writer prj and run the program, but i get below error:
*********************************************************
[ARM9_0] Starting OMAP-L138 NORWriter.
CFI Query...passed.
NOR Initialization:
Command Set: AMD
Manufacturer: INTEL
Size: 0x40 MB
Enter the binary AIS application file name (enter 'none' to skip):
C:\Users\yq1003\DATA\DSP\Code\u-bootais.bin
INFO: File read complete.
Erasing the NOR Flash
Address out of range ERROR: Erasing NOR failed.
NOR flashing failed!
********************************************************
2. After using Nor writer failed many times and i try to use the sfh_OMAP-L138 to flash the Nor flash. First i download the OMAP-L138_FlashAndBootUtils_2_40 and change the DEVICE_UART_PERIPHNUM to 1 ( for i use Uart1), change the Uint32 DEVICE_ExternalMemInit() 5 DDR setting, (for my external clk is 25MHz) change the DEVICE_PLL0Init() and DEVICE_PLL1Init. Then i copy the folder OMAP-L138_FlashAndBootUtils_2_40 to my virtual Ubuntu system. In Ubuntu , go to the \OMAP-L138\GNU , then input "make" and "enter" to build this file. After that i get a new sfh_OMAP-L138.exe. When i use the sfh_OMAP-L138.exe to flash the board, the process stoped at: " Waiting for SFT on the OMAP-L138..."
Any idea please share with me . Thanks