This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x POH Reliability Data for Nitro version

Other Parts Discussed in Thread: AM3352

Hi,

Our customer wants to use 1GHz version of AM3352 in their industrial application.
And the required temperature range is -40°C to 90°C(industrial).

We are confused there there is no option of device selection for
1GHz(nitro) @ Industrial temperature range.

The only option we have is to choose Extended (-40°C to 105°C)
in which case the Lifetime(POH) is reduced to extremely low (37K).

Which indirectly means we cannot choose AM335x (1GHz) for industrial applications.


Best Regards
Kummi