Other Parts Discussed in Thread: CCSTUDIO
Hi,
I try to build the TestAppEncoder of G.711 codec contained in the DVSDK but it doesn't succed. Is because I use CCSv4? (The test application is developped in CCSv3). When finish to import the project and to build it, i get this following:
///////////////////////////////////////
'Building file: C:/TI/dvsdk_wince/dvsdk_wince_1_00_00_05/cs1omap3530_1_00_01/packages/ti/sdo/codecs/g711enc/app/Client/Test/Src/alg_malloc.c'
'Invoking: Compiler'
"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c6000/bin/cl6x" --cmd_file="C:\TI\dvsdk_wince\dvsdk_wince_1_00_00_05\cs1omap3530_1_00_01\packages\ti\sdo\codecs\g711enc\app\Client\Build\TestAppEncoder.cmd" -mv6400+ -g --include_path="C:/Program Files/Texas Instruments/bios_5_41_02_14/packages/ti/bios/include" --include_path="C:/CCStudio_v3.3/C6000/xdais/src/api/" --include_path="C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c6000/include" --include_path="C:/TI/dvsdk_wince/dvsdk_wince_1_00_00_05/cs1omap3530_1_00_01/packages/ti/sdo/codecs/g711enc/app/Client/../Inc" --quiet --diag_warning=225 --src_interlist --temp_directory="C:/TI/dvsdk_wince/dvsdk_wince_1_00_00_05/cs1omap3530_1_00_01/packages/ti/sdo/codecs/g711enc/app/Client/Build/Obj" --asm_directory="C:/TI/dvsdk_wince/dvsdk_wince_1_00_00_05/cs1omap3530_1_00_01/packages/ti/sdo/codecs/g711enc/app/Client/Build/Obj" --obj_directory="C:/TI/dvsdk_wince/dvsdk_wince_1_00_00_05/cs1omap3530_1_00_01/packages/ti/sdo/codecs/g711enc/app/Client/Build/Obj" --preproc_with_compile --preproc_dependency="alg_malloc.pp" "C:/TI/dvsdk_wince/dvsdk_wince_1_00_00_05/cs1omap3530_1_00_01/packages/ti/sdo/codecs/g711enc/app/Client/Test/Src/alg_malloc.c"
>> WARNING: invalid compiler option -tack (ignored)
-heap,--heap=size Specify heap size for C/C++ dynamic memory allocation
'Finished building: C:/TI/dvsdk_wince/dvsdk_wince_1_00_00_05/cs1omap3530_1_00_01/packages/ti/sdo/codecs/g711enc/app/Client/Test/Src/alg_malloc.c'
' '
'Building target: C:/TI/dvsdk_wince/dvsdk_wince_1_00_00_05/cs1omap3530_1_00_01/packages/ti/sdo/codecs/g711enc/app/Client/Build/Out/TestAppEncoder.out'
'Invoking: Linker'
"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c6000/bin/cl6x" -@ccsLinker.opt -o "C:/TI/dvsdk_wince/dvsdk_wince_1_00_00_05/cs1omap3530_1_00_01/packages/ti/sdo/codecs/g711enc/app/Client/Build/Out/TestAppEncoder.out"
-heap,--heap=size Specify heap size for C/C++ dynamic memory allocation
>> WARNING: invalid compiler option -tack (ignored)
'Finished building target: C:/TI/dvsdk_wince/dvsdk_wince_1_00_00_05/cs1omap3530_1_00_01/packages/ti/sdo/codecs/g711enc/app/Client/Build/Out/TestAppEncoder.out'
' '
Build complete for project TestAppEncoder
/////////////////////////////////////////////////////
so It seems it buid completly the project but I can't load the file TestAppEncoder.out on the target because it's not present in the path that's specified (TestAppEncoder.out is not created).
So is anyone already focus this kind of problem? How can I fix it?
Thank you for your help.