Other Parts Discussed in Thread: AM3517
Hi, I'm working with an AM3517 EVM Development Kit. I'm having trouble when connecting the Application board to the EVM, I get the following message:
Texas Instruments X-Loader 1.45 (Mar 19 2010 - 19:44:22)
Starting X-loader on MMC
Reading boot sector
214940 Bytes Read from MMC
Starting OS Bootloader from MMC...
Starting OS Bootloader...
U-Boot 2009.11 (Mar 19 2010 - 19:46:20)
OMAP34xx/35xx-GP ES1.0, CPU-OPP2 L3-165MHz
AM3517EVM Board + LPDDR/NAND
I2C: ready
DRAM: 256 MB
NAND: No NAND device found!!!
0 MiB
As you can see I have the x-loader and the uboot image on an SD card, I have also tried flashing the x-loader and the uboot in NAND with the same result everytime I connect the Application board. It's odd since I get no trouble when I don't attach the application board (I get the uboot prompt and can actually complete the installation kernel and boot from NFS). I've tried using the x-loader and uboot images from PSP 3.00.00.03, and the latest release 3.00.00.05 so far with the same results. Don't know at this point if it is hardware related or what am I missing.
Any help would be much appreciated.
Regards
Diego Chaverri