Other Parts Discussed in Thread: SYSBIOS
Hello ,
We are working on the DM8148 target .
Half a year a go i manged to build and run the IPC example MsgQ_02 on Windows host with CCS 5.x .
Since i wanted to work with UIA and i read in E2E that it is recomended to move to CCS6 to be more freindly
i moved to CCS6 , also moved to Linux Host .
I am trying to build the IPC example MsgQ_02 on the DSP side in CCS6 and do not suceed .
1. Is there an IPC version that works with XDCTOOLS versions 3.30.xx ?
2. Where can i find sets of IPC , SYSBIOS , UIA and XDCTOOLS versions that works togethere ( and if tested onlinux ) .
3. When i am creating new Platform in the wizard and the XDCTOOS in windows->preference->ccs->rtsc is set to 3.30.xx
i get errors at the end and only after i change the XDCTOOLS to 3.23.xx version at the above location it manages to save it .
why is that ?
4. And also when i manage to create a new platform i can not see it in the 'Platform' Drop down list in RTSC dialog in project properties .
How this list of platforms is built i try to but did not understand .
5. I work with CCS6 version 6.0.1.00039 , should i move to version 6.1.xx ?
Regards , Shlomo .