This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to route data via DSP Board ?



hello every body,  I am working on DM648 with ndk1.92. I want to implement an intelligent switch application with the involvement of DSP processor of the topology mentioned below

   data from LAN ----->port0 (PHY 1) of dsp ------>port2( DSP processor) --------->port1(PHY 2) --------> to the PC

and similarly

To LAN <-----port0 (PHY 1) of dsp <------port2( DSP processor) <---------port1(PHY 2) <-------- data from PC

in a full duplex fashion. Now could u plz guide which NDk program i.e (cfgdemo,client , hello world or anyother ) should I use.

I had tried alot on helloworld application but it has been configured in normal mode(i.e data do not go to DSP ) do anybody know how to configure it in bypass mode?

Note that I do not need  DHCP,HTTP or any other server client application out of it.

Waiting for ur reply

Regards

Ahmed