Hello,
I would like to ask about deinterlacer:
Does anyone knows what it means if input and output rate is configured the same value in deinterlacer, which is supposed to work in deintralce mode (interlace->progressive).
I have an issue where fast camera movements are displayed in jumps in the display, so on changing parameters, I notices that when dei input frame rate is configured same value as output frame rate, then the behaviour is much better,
Regards,
Ran