I am new to the Audio related stuff : need help : any one please help me this --
From AM335x ACLK, FSX, AXR2, AXR3 are connected to Audio DAC - TLV320DAC3100 -- which is having headphone 3.5 jack and speaker.
AM335x - of -- ACLK -to - BCLK -of- codec
FSX -- FSX - codec
AXR2 -- DIN -- codec
AXR3 -- Dout -- but not connected -- left it as Test Point
CLKOUT1 -- MCLK of Codec // i forgot this pin -- need to do pin muxing -- for this IO as CLOCK.
in the the device tree
op-mode = <0>; /* MCASP_IIS_MODE */ -- do we need to change the parameters here op-mode
tdm-slots = <2>;
/* 4 serializers */
serial-dir = < /* 0: INACTIVE, 1: TX, 2: RX */ -- here i am having doubt -- is this parameter is correct
1 0 0 0
>;
Regards,
Viswanath K.