Hello Support/Fellow Engineers,
I am new to this forum and wish to use the TMS320C5505 with a stereo CODEC sampling 2 channels/Stereo 96kHz sampling 24 bit, (ie 768kBytes/s 32bit) writing data as a wav file an SD card using the SD/MMC-4bit SDIO port using a FAT File system. I expect I will also use the external memory either via the EBI i/f to SDRAM or Async SRAM for buffering whilst writing to the SD card 50MHz.
Please confirm if this part can perform this task or recommend an alternative.
With kind regards,
Ramesh