Hello,
I would please like to ask the following question, it is issue I had for a long time now, and fixed it with a workaround.
If I record file without the starting it with I-frame, than trying to decode-display the file result in errors and eventually nothing is displayed:
[m3video] 58864:DECLINK::links_m3video/iva_dec/decLink_h264.c:[378]::INTERNAL ERROR:-1
…
I "fixed" it by waiting to the first I-frame, and only then starting to fill into the file (so that file always start with I-frame).
This workaround is problematic because the decode-display should handle also stream which does not begin with I-frame, especially if it comes from network.
I would like to ask how I can handle this issue properly ?
This is a link for the test file with non I-frame at the beginning:

Thank you!
Ran