Hello,
I'm trying to learn about the various topology/configuration options of DDR3 memory.
For example, please review the following document:

At page 11, table 2. second row - you see:
1Gb / (8M × 16 × 8) × 2 SDRAMs
As I understand it:
1Gb - is the total size of the on chip memory.
8M - is the size of each memory sub array inside the chip.
16 - is the number of banks.
8 - is the number of arrays per bank.
2 - is the number of SDRAM chips per memory rank
Is my observation correct?