This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI Flash using Uniflash on AM335x EVM SDK 8.0

Other Parts Discussed in Thread: UNIFLASH

Hi 

We are trying SPI flash on AM335x EVM using uniflash utiliy.

We are working on SDK 8.0.

Referred following link

http://processors.wiki.ti.com/index.php/Sitara_Linux_Program_SPI_Flash_on_AM335x_EVM

This link is with the referece of SDK 6.0 ( The patches mentioned for u-boot)

1. We would like to know the changes in SDK 8.0 u-boot code to be done to support SPI flash  and to use the uniflash utility.

2. To Set the EVM to boot from the appropriate interface , The sysboot pins configuration for USB is missing , only for Ethernet interface its present.

It will be good if any input regarding SPI flash using uniflash on AM335x EVM with SDK 8.0

Regards,

Nagaraj