Other Parts Discussed in Thread: OMAP-L138
I have been using an in-house prototype that was L137 based - that is up and running (all in-house code - no Linux or DSP/BIOS...)
I just received the first sample of a newer prototype board that has L138 and DDR2 instead of L137 and SDRAM and I'm having some problems getting anywhere.
Questions:
1) Where do I get GEL files for L138 (I see references to c6748.gel on the forums - but I do not have it...)
2) If I leave CCS configured for my L137 based prototype board it will connect to the DSP - but connecting to the ARM gives me
Trouble Halting Target CPU: Error 0x00000020/-2011 Error during: Execution, An internal error occurred in which an illegal action (0x00000000) was requested while disconnected.
about a dozen times...Which could easily be due to some configuration issue - or to the fact that it is trying to boot from NOR flash - and the flash is not initialized...
(I kind of need to get into the processor with the JTAG to update the flash.....)
Ken Dougherty