This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ECG Implementation on the TMS320C5515E DSP Medical Development Kit with the ADS1298 ECG-FE

I'm not able to run tutorial "Running ECG Demo application on the C5515 EVM" as in your Application Report SPRABJ1-January 2011 with CCS4  Version: 4.1.0.02002  (not.CCS3.3 as suggested in application note SPRABJ1)

Following instructions i can't find file ECGSystem.pjt in "ADS1298ECGSystem_v1.12" folder downloaded fro http://code.google.com/p/c5505-ezdsp/  and i obtain different behavior compared with description in your report at "debug-launch" using ECG_NonBIOS.pjt.

Please send me instructions for run ECG demo Application

  • Hi,

    What is the error you are getting ?

    I tried to build the same using CCS 5.5 version and I was able to build this successfully.

    When I imported the project,  I selected "legacy CCS3.3 project " as an option and then need to add the following in my include path - " <>:\ti\bios_5_41_13_42\packages\ti\bios\include "

    I do not think "ECGSystem.pjt" exists looks like they are pointing to ECG_NonBIOS.pjt .

    Hope you can try with the above mentioned option and it works.

    Regards

     Vasanth

  • I'll trie next week

    thanks for suggest

    Stefano