Hi,
I'm trying to use the writeback to produce a progressive video output from a video entry that has the video timings set to interlaced video. My scheme consist basically in a video output with the timing configured to deploy 1080i and then use the writeback to capture back from that port; the problem I have is that when I try to use the writeback on that output I'm only able to obtain one field in each buffer. My question is, is there any way I can capture both fields in the same buffer? ie is there any method for having the writeback merging fields ?