Hi
I am trying to a sample OpenGL ES code which just draws a triangle on screen. I need to read back the display buffer content, so I used glreadpixels. But it is always filling my buffers with zeros. I have referred to http://processors.wiki.ti.com/index.php/Render_to_Texture_with_OpenGL_ES.
I am not rendering to any FBO. I am using the window system created framebuffer and default GL_COLOR_ATTACHMENT0.
My render code looks like this:
glClearColor(0.5, 0.5, 0.5, 1.0); glClear(GL_COLOR_BUFFER_BIT); glDrawArrays ( GL_TRIANGLES, 0, 3 ); glReadPixels(0, 0, width,height, GL_RGB,GL_UNSIGNED_BYTE,pixels); eglSwapBuffers(gl.display, gl.surface);
My fragment shader :
void main()
{
gl_FragColor = vec4 ( 1.0, 0.0, 0.0, 1.0 );
}
My vertex shader
void main()
{
gl_Position = vPosition;
}
with the following vertices:
GLfloat vVertices[] = { 0.0f, 0.5f, 0.0f,
-0.5f, -0.5f, 0.0f,
0.5f, -0.5f, 0.0f };
My rendering is working properly.
Why is glReadPixel always filling buffer with zeros?.
Thanks & Regards
Thushara