This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP AM37x sleep mode / clock debugging

We have a custom board with an AM37x, we're running Linux 3.10 from the Android open source project, OMAP branch. 

My problem is in getting the device to idle / sleep at the deepest stage. It goes through stages 1-6, but refuses to enter state7. I've done all the usual fixes: set enable_off_mode to 1, disabled UART as a wake-up source and removed drivers. Still, the core and PER power-domains won't sleep.

I use "echo mem > /sys/power/state" for testing. Upon wake, I get warnings that PER and core didn't enter the targeted power-state. 

As I understand it, PER and core are co-dependent for sleeping. I suspect that either holds a clock that isn't disabled.

So, I have several questions - first, am I missing something obvious? Is a clock the likely culprit? If so, what is the best way to find which clock is the problem? There are lots of clocks in use. Are there other things that would keep one of these domains awake?

I have the Clock Tree Tool for my chip (although that's for ES1.0, we're ES1.2) - is there an easy way to create a register dump that I can load into the clock tree tool?

Any advice appreciated.

  • Hi Mattis,

    This forum supports only the TI distributed Linux SDK, which is currently kernel v2.6.37 for the AM37X (http://software-dl.ti.com/sitara_linux/esd/AM37xSDK/latest/index_FDS.html ). I will ask the SW team to help on the CTT question.

  • Hi Mattis, 

    Mattis Fjallstrom said:
    So, I have several questions - first, am I missing something obvious? Is a clock the likely culprit?

     

    It is also possible that some module (IP in the core or PER power domain) you use is stuck in transition between power stages. The best approach for debugging is to use minimal rootfs & minimal config, disable every possible driver & then add things back one by one, to see what is breaking the suspend/resume sequence.

    Mattis Fjallstrom said:
    I have the Clock Tree Tool for my chip (although that's for ES1.0, we're ES1.2) - is there an easy way to create a register dump that I can load into the clock tree tool?

    It is possible to load register settings in the clock tree tool. You need to create a dump from the kernel in the form: 
      <register address>    <register value> 

    save the file as .rd1  & load it in CTT. 

    Best Regards, 

    Yordan