I use the 3PSW Ethernet Subsystem on DM648 on my custom board with the following configuration settings.
REFCLKP/N:62.5 MHz, MPY: 20x, RATE: Half making the Line rate to 1250MHz.
Is 1250MHz the max possible line rate acheivable on DM648? I know that the multiplier can be set to a max value of 25x and REFCLK to 125MHz and RATE to Full. But not sure the DM648 will work in this combination of settings..
Also, currently the DM648 in my application receives a maximum payload size of 1472 bytes per packet (excluding the protocol headers) from host to which it is connected over ethernet. Does DM648 support receiving packets greater than 1500 bytes?
SP