Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

U-Boot & SATA

Hello,

I've new custom L138 -based board with SPI-FLASH, I2C-EEPROM and SATA-SSD. I would very much like to boot system from either FLASH or EEPROM with AIS including U-Boot  which would then initialize kernel and file system from SSD. 

Does U-Boot from mcsdk_1_01_00_02/board-support/u-boot-2012.04.01-psp03.22.00.06.sdk support SATA? Is there excisting L138-U-Boot supporting SATA or how do you recommend this to be realized?

Best Regards,

risto