Hi,
I have a question about EDMA3LLD for C6670.
In my system, I use multiple coprocessor which are supported by C6670.
For example, I use VCP2 and TCP3D co-processor which both uses EDMA3.
My question is about EDMA3 initialization. In EDMA3LLD, there is edma initialization function edma3init().
Q1.Does edma3init() need to be executed twice for each VCP2 and TCP3D?
Q2.Or should edma3init() be executed only once by making common edma3init()?
Q3. If executing edma3init() not twice but once is must,
are there any sample program of multiple co-processor with EDMA3?
best regards,
g.f.