This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

using 320c5515 as a Microphone limiter and graphic equalizer at 1.1V supply with very limited current



Hi Guy´s,

Are trying to see if possible to use the above 320c5515 do do my wanted function.

I would like to have a microphones signal to pass through a DSP that works as a limiter in stage 1 ( so that the connected units mic-inlet not get overloaded,read distorted)

and at the same time I would like to change the microphones signal with an Graphic equalizer in stage 2 of the processline, so that I can make the picked up voice to be the way I like it to be.

What do I need, or do you have a better idea for Another Circuit that could work for me.

My biggest problem is that it is intended to be connected to a mobile phones microphone inlet, and the voltage normally is not over 1.1V and the given current is around 1mA. And  would like to avoid to have an external Power source.

Best Regards

Bo Franzen bo@neckmike.com