This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335XEVM - fastboot does not see the device

I am trying to use fastboot (on a 32bit Windows7) to update the EMMC firmware but fastboot is not seeing my device.

I have installed fastboot on the pc and have also installed the driver for the AM335xevm.  The Device Manager properties showed "this device is working properly"

with USB\VID:   USB\VID_0451&PID_D022

 

Device Manager showed:

     Universal Serial Bus devices

        AM335xevm

   

On power-up, I hit "enter" a few times and was able to get into "U-Boot#", I then typed in "fastboot" and got

mmc_send_cmd :  timeout:  No status update

mmc1(part 0) is current device

mmc_send_cmd :  timeout:  No status update

Loading efi partition table:

             256        128k  spl

             512        512k  blootloader

and so on,,,,,

Fastboot entered .....

musb-hdrc:  peripheral reset irq lost!

 

Then on different command window where abd.exe and fastboot.exe are located, I typed "fastboot devices" and got nothing.

I have also tried "fastboot oem format" and got < waiting for devices >

 

When the device is NOT is "fastboot" mode, adb is working fine, I can issue "adb devices" and got:

0123456789ABCDEF    devices