This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCI6636 repeat loading BIOSdemo problem

 have done about the TCI6636 card via srio API to send and receive data on test, demo is now running on TCI6636 a BIOS enumeration and send works, would like to ask, can separated into two BIOS enumeration and sending demo, first run an enumeration, built after the routing table, find the target ID that is sent, and then modify the sent works, Reload send demo go to TCI6636 to run, right? Now don't realize is you have loaded two at TCI6636 BIOS demo, do you need any modification to the program initialization?

  • Hi,

    Welcome to the TI E2E forum. I hope you will find many good answers here and in the TI.com documents and in the TI Wiki Pages (for processor issues). Be sure to search those for helpful information and to browse for the questions others may have asked on similar topics (e2e.ti.com). Please refer all the links below my signature. 

    Are you working on EVM or Custom board? Are you working on MCSDK example? What is the MCSDK version used?

    Thank you.

  • Can be understood as EVM Board, not the MCSDK demo, but is based on the MSCDKdemo and development, MCSDK version is mcsdk_bios_3_01_01_04, I just wanted to know if I can repeat loading BIOS on TCI6636 the demo, what needs to be done

    thank you very much.

  • Hi Shengfeng,

    Your question is not very clear. I am guessing you want to know if it is okay to reload the SYS/BIOS application and if there are any special requirements to do so. The answer is yes, it is okay to reload the application and you dont need to do any special configuration in the application. When the application is loaded again, it will go through the cinit phase which will initialize the data sections.

    Best,
    Ashish

  • sorry,My English is not good, it is possible to describe is not clear. According to you of answered TCI6636 is can again loaded BIOS program of, but now I encountered of problem is, I wants to in TCI6636 Shang first run routing table program, to chassis in the each srio equipment distribution a ID,, then again run a sent program, this inside has a problem is, if again run has BIOS of sent end program, will again initial of, so long cannot found corresponds to of ID has?
  • Hi Shengfeng,

    I am sorry but I am still having a hard time understanding the question. Can you try using google translator (https://translate.google.com) to translate your question from your native language to english ?

    Thanks,
    Ashish