Other Parts Discussed in Thread: TMS320C6748, TMS320C6742, AM1808, TMS320C6474, OMAP-L138
We are using TMS320C6748 DSP in our design and want to know following details,
1. In the html page of Power Requirements for TMS320C6742/C6746/C6748,
(a) VDDARNWA, VDDARNW1 pins are mentioned. which DSP has these pins? Because those pins are not there in C6748.Please clarify on this?
(b) For the similar pin group the current requirement is mentioned as 200mA in html page and 250mA in another pdf file(Application Report-slva340).What is exact curent requirement for TMS320C6748?Please clarify on this.
2.If we are not using SATA and USB1 modules can we leave the SATA_VDD, SATA_VDDR and USB1_VDDA18, USB1_VDDA 33 pins unconnected?
3.For DDR2SDRAM controller’s data (I/O) bus, one series termination at DDR2 module is shown in the datasheet high-level schematic in page no.106 of C6748. Please let us know whether one termination(at DDR2 side) is sufficient or whether series termination is required at both source(DSP ) and destination(DDR2) end?
4.Please let us know whether any excel sheet for power calculation of TMS320C6748 is available.
Regards
Deelip