This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM6678 SRIO stabilization time

Hi

My customer has one SRIO question on custom board.

There are three DSP on the board and one DSP is connected to two other DSP with SRIO like below.

             DSP1 <- x1 ->DSP2 <- x1 -> DSP3

1. DSP1/2/3 initialize SRIO port and wait some time(about 10 seconds).
2. DSP2 starts to send test data to DSP1/3 after waiting time.
3. And DSP1 and DSP3 re-send received data to DSP2.
4. Then DSP2 compares data from DSP1/3 with its test data.

The problem is that the reply time is very variable.
It takes 1 ~ 3 minutes for DSP2 to receive data re-sent by DSP1/3.

Can you let me know how long it takes to start transmission on two EVM?

Regards,

YC