This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x XIP boot image Detection



The section 26.1.7.2 on SPRUH73L describes:

"The boot procedure from XIP device can be described as such:

 ・ Configure GPMC for XIP device access.

 ・ Set the image location to 0x08000000.

 ・ Verify if bootable image is present at the image location.

 ・ If the image has been found, start the execution.

 ・ If the image has not been found, return from XIP booting to the main booting loop."

How is the boot image verified by the ROM Code?

Best regards,

Daisuke