Hi,
I'm using TI-RTOS version "tirtos_tivac_2_10_01_38" and i migrated to "tirtos_tivac_2_12_01_33" and compiler v5.2.4 for TM4C129 controller that run on the DK129.
i have many devices on the SPI interface and i'm using SPI with DMA for TIVA, but i noticed that for unknown reason the processor is stucking during sending for no reason, and i noticed that this version of the TI-RTOS has the following fix,
| SDOCM00114670 | S2 - Major |
SPI driver for Tiva is spinning in the hwi for TivaC but not for snowflake |
So, is fix generating another problem?
also i noticed that the task which is responsable to do the SPI transfere is blocked on unkown!!!
Thanks,
Mohamed