This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x Signal Transition Levels for timing parameters



Are all input and output timing parameters referenced to 50% I/O voltage for both "0" and "1" logic levels?

Are all rise and fall transition timing parameters referenced to VIL MAX and VIH MIN for input clocks, VOL MAX and VOH MIN for output clocks?

Best regards,

Daisuke