This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 NAND FLash Burn with Single Image

Hi,

This is Bobby from AudioCodes company.

I am working on the EVB board basing on EZSDK of "ti-ezsdk_dm814x-evm_5_05_02_00", Per each testings are ok.

Now, I am trying to change the filesystem from jffs2 to UBIFS, because the JFFS2 image will cause a issue of broken block when working on NAND FLASH(SD card work fine).

But now, it is so trouble to program so many images (by command "nand write.i" and "mw.b" in bootloader stage), such as "u-boot.min.nand", "u-boot.bin", "uImage" and more, can I generate a single image(such as *.img or *.rmt) to program to NAND flash, it will help factory usage very much!

Would you tell me how to implement it? It is so rushed due to the factory pushed me everyday.

Thanks you very much!

Best Regards,

Bobby