Hi,
I want to clear the bus of I2C of DM8168 because a peripheral is driving SDA bus low.
I find the following web site.
lists.infradead.org/.../080062.html
Can the I2C_SYSTEST register of DM8168 use it in the same way, too?
The[5..0]bit of the I2C_SYSTEST register of Table 21-33 of TRM of DM8168 has a mention like read-only, is it an error in writing?
Judging from contents of description, SDA_O bit and the SDL_O bit are thought to be writable.
Best Regards,
Shigehiro Tsuda