I use the DVRRDK 04.01.00.02 on a custom board with a DM8107.
I try to capture two video simultaneously. the first in 1080p25 on VIP0 port A and the second in 720p50 on VIP1 port A.
My usecase is :
VIP0 and VIP1 --> DEI --> NSF --> ENC
My problem is that it seem that the lane where I capture the video in 1080p25 is cropped in 720p.
The result is this :
The video captured and encodede in 720p is good.
The log of my application :
These informations in the log seems to me strange. I have also tested without DEI but I have always the problem.
An idea ?
Regards