Hello,
I'm working with DSP TCI6487 or TCI6488 according to the reference of our boards. Does it exist some registers inside the DSP to be read to determine :
- if DSP is 6487 or 6488
- if device speed max is 1 GHz or 1.2 GHz
If not, what is the software way to access to these nomenclature information ?
The goal is to be able to configure PLL registers to enjoy the max speed.
Thanks in advance for your support
Olivier