linux kernel initializes k2h's peripherals (srio, hyperlink, pktdma, nwal..) on the arm boot mode.
i faced the problem k2h device initialization is duplicated
while arm kernel is runnung because and examples have init codes and run too.
i think that arm's or dsp's side specific init codes are needed to block to prevent duplication.
but i want to init codes are done only dsp side because there are some parameters whose values are modified.
is this possible to initialize peripherals only dsp side while linux kernel whose specific devices are blocked is running?