Hi,
I know the evm66ak2h Image Processing example code is provided in mcsdk_bios_3_01_03_06/demos/image_processing/ipc.
But the IPC example is not there.
In fact. the two IPC and image processing examples launched by the Matrix Application Launcher are located in different places in the rootfs. The image processing demo code is found in /usr/share/apps/demo_imageproc/bin & cgi-bin, while the IPC code is located in /lib/firmware/
IPC_3_35 provides IPC examples for various processors, but not evm2k / ARM (?).
Where do I find the IPC example code provided with the EVM.
Also, you need to revise your MCSDK Image Processing Demo Guide for Keystone II, which states that the MCSDK provides a Serial-based demo, an IPC-based demo and OpenMP-based demo. MCSDK_3 only provides the IPC-based demo. (The other versions appear in MCSDK_2.)
Regards,
Bernard