Dear Sir,
I bought the DVR RDK 8168 from udworks and version 4. Can you mail me that which file has memory mapping address list in linux source code such as nand flash, ddr3, ethernet, usb and etc?
Regards,Balaji
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
I bought the DVR RDK 8168 from udworks and version 4. Can you mail me that which file has memory mapping address list in linux source code such as nand flash, ddr3, ethernet, usb and etc?
Regards,Balaji
Hi Balaji,
See files
linux-kernel/arch/arm/plat-omap/include/plat/ti81xx.h
linux-kernel/arch/arm/plat-omap/include/plat/io.h
linux-kernel/arch/arm/mach-omap2/devices.c
BR
Pavel