This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with the Emulation Controller

Hi,

Can somebody decode these errors? Why these errors occur and how to fix them?

C55xx: Error: Error 0xA0002020/-1041 Error during: Execution, Control, Device driver: Problem with the Emulation Controller. It is recommended to RESET EMULATOR. This will disconnect each target from the emulator. The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target.

C55xx: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging

Thanks.

Regards,

VJ

  • Two more errors to seek explaination for

    C55xx: Error connecting to the target: Error 0x80000240/-151 Fatal Error during: Initialization, OCS, This error was generated by TI's USCIF driver. SC_ERR_POD_OPEN <-151> This utility failed to open the adapter for a custom emulator. The adapter returned an error.

    C55xx: Error connecting to the target: Error 0x80002240/-121 Fatal Error during: Initialization, OCS, Control, This error was generated by TI's USCIF driver. SC_ERR_CMD_HANDLE <-121> A bad controller handle has been given to a function, either before attempting to open the controller, or after having opened the controller and ignored its error status. Valid controller handles are generated when attempts to open the controller return a clean error status.

    Awaitng reply.

    Thanks.

    VJ

  • Please focus on your signal DSP_RESET and check your reset IC.