Hi to everyone,
We are working on TMS320C6670 DSP. The custom platform project was created in the CCS 5.5 that has next files:
.cproject
.project
config.bld
package.bld
package.xdc
Platform.xdc
Platform.xs
As I know this is all the necessary files to build a binary platform from it. So when I do File->Import->Existing project to the Workspace it attached and building just fine. Bu the problem is that the project cannot become Active in the CCS 6 environment, also Clear project feature doesn't work. So after hitting the "Clean Project" nothing happens. There is no such problem in the CCS 5.5. Any idea how to fix this?
Best Regards,
Pavlo!