This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

reset DSP with WDT reset

Hi,

I use DM8168, with linux 2.6.37 coming from arago (http://arago-project.org/git/projects/?p=linux-omap3.git;a=commit;h=1d061a793577359bcc7fe9007d221e8028ba1a8f).

When WDT trigger a reset it seems that DSP isn't reset itself.

How to make DSP reset when WDT trigger a reset?

best regards

Max

  • Hi Max,

    mastupristi said:
    When WDT trigger a reset it seems that DSP isn't reset itself.

    How exactly you define that C674x DSP core is not reset by the WDT? In DM816x datasheet (8.2 Reset) is stated that WDT resets everything except Emulation logic and do not latch sysboot pins.

    See if the below resources will be in help:

    DM816x silicon errata, Advisory 1.1.37 and Advisory 2.1.65



    BR
    Pavel