This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

StarterWare public repository with bugfixes and enhancements



Hello everybody,

since further development of StarterWare for AM335X seems to stall, we decided to create a public repository everybody can use and that contains enhancements, bugfixes and improvements that never became part of t TI's original package. The repository is available at https://sourceforge.net/projects/starterwarefree/ , the sources are available in GIT to be found at https://sourceforge.net/p/starterwarefree/code/ci/master/tree/ . What we have at the moment:

  • BeagleBone Black patch included
  • several bugfixes included (as reported here in forum)
  • additional support and driver functions
  • base implementation for MMC access
  • functions and definitions for PRU usage
  • FatFS 0.10b
  • lwIP switched back to original version 1.4.0 (without these strange modifications that come with StarterWare)

This repository of course can't live without the help of a community. So we're looking for people that are interested in getting involved, in supporting this code repository and in contributing to it.

Thanks

Jim

  • I checked out the repository and it looks really good! There are a lot of bugfixes in there TI never published in an official release. So...how can one become part of the development team there?

  • I'd like to have that as uncomplicated as possible:

    • send me a patch with some enhancements/bugfixes/whatever useful changes
    • send me your sf.net username
    • when the patch looks good, I add you to the active developers with write access to the repository so that you can apply your modifications

    There are also some development rules available in Wiki.

    Btw: the project needs some additional developer,s I can't handle everything for my own, so whoever is interested in taking part at development, please let me know!

    Jim

  • Great, I'll contact you via SF.net mail!

  • Greetings Jim:

    I have downloaded the project from SF and patched it into my existing starterware project folders. So far I like the looks of what you have done.

    It appears as if the file third_party\fatfs\src\ffconf.h is missing from SF.

    Respectfully,
    David

  • You are right, it got lost somehow - thanks for the information!

    It will be added to the repo, please find it attached to this posting too:

    /*---------------------------------------------------------------------------/
    /  FatFs - FAT file system module configuration file  R0.10b (C)ChaN, 2014
    /---------------------------------------------------------------------------*/
    
    #ifndef _FFCONF
    #define _FFCONF 8051	/* Revision ID */
    
    
    /*---------------------------------------------------------------------------/
    / Functions and Buffer Configurations
    /---------------------------------------------------------------------------*/
    
    #define	_FS_TINY		1	/* 0:Normal or 1:Tiny */
    /* When _FS_TINY is set to 1, it reduces memory consumption _MAX_SS bytes each
    /  file object. For file data transfer, FatFs uses the common sector buffer in
    /  the file system object (FATFS) instead of private sector buffer eliminated
    /  from the file object (FIL). */
    
    
    #define _FS_READONLY	0	/* 0:Read/Write or 1:Read only */
    /* Setting _FS_READONLY to 1 defines read only configuration. This removes
    /  writing functions, f_write(), f_sync(), f_unlink(), f_mkdir(), f_chmod(),
    /  f_rename(), f_truncate() and useless f_getfree(). */
    
    
    #define _FS_MINIMIZE	0	/* 0 to 3 */
    /* The _FS_MINIMIZE option defines minimization level to remove API functions.
    /
    /   0: All basic functions are enabled.
    /   1: f_stat(), f_getfree(), f_unlink(), f_mkdir(), f_chmod(), f_utime(),
    /      f_truncate() and f_rename() function are removed.
    /   2: f_opendir(), f_readdir() and f_closedir() are removed in addition to 1.
    /   3: f_lseek() function is removed in addition to 2. */
    
    
    #define	_USE_STRFUNC	0	/* 0:Disable or 1-2:Enable */
    /* To enable string functions, set _USE_STRFUNC to 1 or 2. */
    
    
    #define	_USE_MKFS		0	/* 0:Disable or 1:Enable */
    /* To enable f_mkfs() function, set _USE_MKFS to 1 and set _FS_READONLY to 0 */
    
    
    #define	_USE_FASTSEEK	0	/* 0:Disable or 1:Enable */
    /* To enable fast seek feature, set _USE_FASTSEEK to 1. */
    
    
    #define _USE_LABEL		0	/* 0:Disable or 1:Enable */
    /* To enable volume label functions, set _USE_LAVEL to 1 */
    
    
    #define	_USE_FORWARD	0	/* 0:Disable or 1:Enable */
    /* To enable f_forward() function, set _USE_FORWARD to 1 and set _FS_TINY to 1. */
    
    
    /*---------------------------------------------------------------------------/
    / Locale and Namespace Configurations
    /---------------------------------------------------------------------------*/
    
    #define _CODE_PAGE	858
    /* The _CODE_PAGE specifies the OEM code page to be used on the target system.
    /  Incorrect setting of the code page can cause a file open failure.
    /
    /   932  - Japanese Shift_JIS (DBCS, OEM, Windows)
    /   936  - Simplified Chinese GBK (DBCS, OEM, Windows)
    /   949  - Korean (DBCS, OEM, Windows)
    /   950  - Traditional Chinese Big5 (DBCS, OEM, Windows)
    /   1250 - Central Europe (Windows)
    /   1251 - Cyrillic (Windows)
    /   1252 - Latin 1 (Windows)
    /   1253 - Greek (Windows)
    /   1254 - Turkish (Windows)
    /   1255 - Hebrew (Windows)
    /   1256 - Arabic (Windows)
    /   1257 - Baltic (Windows)
    /   1258 - Vietnam (OEM, Windows)
    /   437  - U.S. (OEM)
    /   720  - Arabic (OEM)
    /   737  - Greek (OEM)
    /   775  - Baltic (OEM)
    /   850  - Multilingual Latin 1 (OEM)
    /   858  - Multilingual Latin 1 + Euro (OEM)
    /   852  - Latin 2 (OEM)
    /   855  - Cyrillic (OEM)
    /   866  - Russian (OEM)
    /   857  - Turkish (OEM)
    /   862  - Hebrew (OEM)
    /   874  - Thai (OEM, Windows)
    /   1    - ASCII (Valid for only non-LFN configuration) */
    
    
    #define	_USE_LFN	0		/* 0 to 3 */
    #define	_MAX_LFN	255		/* Maximum LFN length to handle (12 to 255) */
    /* The _USE_LFN option switches the LFN feature.
    /
    /   0: Disable LFN feature. _MAX_LFN has no effect.
    /   1: Enable LFN with static working buffer on the BSS. Always NOT thread-safe.
    /   2: Enable LFN with dynamic working buffer on the STACK.
    /   3: Enable LFN with dynamic working buffer on the HEAP.
    /
    /  When enable LFN feature, Unicode handling functions ff_convert() and ff_wtoupper()
    /  function must be added to the project.
    /  The LFN working buffer occupies (_MAX_LFN + 1) * 2 bytes. When use stack for the
    /  working buffer, take care on stack overflow. When use heap memory for the working
    /  buffer, memory management functions, ff_memalloc() and ff_memfree(), must be added
    /  to the project. */
    
    
    #define	_LFN_UNICODE	0	/* 0:ANSI/OEM or 1:Unicode */
    /* To switch the character encoding on the FatFs API (TCHAR) to Unicode, enable LFN
    /  feature and set _LFN_UNICODE to 1. This option affects behavior of string I/O
    /  functions. This option must be 0 when LFN feature is not enabled. */
    
    
    #define _STRF_ENCODE	0	/* 0:ANSI/OEM, 1:UTF-16LE, 2:UTF-16BE, 3:UTF-8 */
    /* When Unicode API is enabled by _LFN_UNICODE option, this option selects the character
    /  encoding on the file to be read/written via string I/O functions, f_gets(), f_putc(),
    /  f_puts and f_printf(). This option has no effect when _LFN_UNICODE == 0. Note that
    /  FatFs supports only BMP. */
    
    
    #define _FS_RPATH		0	/* 0 to 2 */
    /* The _FS_RPATH option configures relative path feature.
    /
    /   0: Disable relative path feature and remove related functions.
    /   1: Enable relative path. f_chdrive() and f_chdir() function are available.
    /   2: f_getcwd() function is available in addition to 1.
    /
    /  Note that output of the f_readdir() fnction is affected by this option. */
    
    
    /*---------------------------------------------------------------------------/
    / Drive/Volume Configurations
    /---------------------------------------------------------------------------*/
    
    #define _VOLUMES	2
    /* Number of volumes (logical drives) to be used. */
    
    
    #define _STR_VOLUME_ID	0	/* 0:Use only 0-9 for drive ID, 1:Use strings for drive ID */
    #define _VOLUME_STRS	"","","","","","","",""
    /* When _STR_VOLUME_ID is set to 1, also pre-defined strings can be used as drive
    /  number in the path name. _VOLUME_STRS defines the drive ID strings for each logical
    /  drives. Number of items must be equal to _VOLUMES. Valid characters for the drive ID
    /  strings are: 0-9 and A-Z. */
    
    
    #define	_MULTI_PARTITION	0	/* 0:Single partition, 1:Enable multiple partition */
    /* By default(0), each logical drive number is bound to the same physical drive number
    /  and only a FAT volume found on the physical drive is mounted. When it is set to 1,
    /  each logical drive number is bound to arbitrary drive/partition listed in VolToPart[].
    */
    
    
    #define	_MIN_SS		512
    #define	_MAX_SS		512
    /* These options configure the range of sector size to be supported. (512, 1024, 2048 or
    /  4096) Always set both 512 for most systems, all memory card and harddisk. But a larger
    /  value may be required for on-board flash memory and some type of optical media.
    /  When _MAX_SS is larger than _MIN_SS, FatFs is configured to variable sector size and
    /  GET_SECTOR_SIZE command must be implemented to the disk_ioctl() function. */
    
    
    #define	_USE_ERASE	0	/* 0:Disable or 1:Enable */
    /* To enable sector erase feature, set _USE_ERASE to 1. Also CTRL_ERASE_SECTOR command
    /  should be added to the disk_ioctl() function. */
    
    
    #define _FS_NOFSINFO	0	/* 0 to 3 */
    /* If you need to know correct free space on the FAT32 volume, set bit 0 of this option
    /  and f_getfree() function at first time after volume mount will force a full FAT scan.
    /  Bit 1 controls the last allocated cluster number as bit 0.
    /
    /  bit0=0: Use free cluster count in the FSINFO if available.
    /  bit0=1: Do not trust free cluster count in the FSINFO.
    /  bit1=0: Use last allocated cluster number in the FSINFO if available.
    /  bit1=1: Do not trust last allocated cluster number in the FSINFO.
    */
    
    
    
    /*---------------------------------------------------------------------------/
    / System Configurations
    /---------------------------------------------------------------------------*/
    
    #define	_FS_LOCK	0	/* 0:Disable or >=1:Enable */
    /* To enable file lock control feature, set _FS_LOCK to non-zero value.
    /  The value defines how many files/sub-directories can be opened simultaneously
    /  with file lock control. This feature uses bss _FS_LOCK * 12 bytes. */
    
    
    #define _FS_REENTRANT	0		/* 0:Disable or 1:Enable */
    #define _FS_TIMEOUT		1000	/* Timeout period in unit of time tick */
    #define	_SYNC_t			HANDLE	/* O/S dependent sync object type. e.g. HANDLE, OS_EVENT*, ID, SemaphoreHandle_t and etc.. */
    /* The _FS_REENTRANT option switches the re-entrancy (thread safe) of the FatFs module.
    /
    /   0: Disable re-entrancy. _FS_TIMEOUT and _SYNC_t have no effect.
    /   1: Enable re-entrancy. Also user provided synchronization handlers,
    /      ff_req_grant(), ff_rel_grant(), ff_del_syncobj() and ff_cre_syncobj()
    /      function must be added to the project.
    */
    
    
    #define _WORD_ACCESS	1	/* 0 or 1 */
    /* The _WORD_ACCESS option is an only platform dependent option. It defines
    /  which access method is used to the word data on the FAT volume.
    /
    /   0: Byte-by-byte access. Always compatible with all platforms.
    /   1: Word access. Do not choose this unless under both the following conditions.
    /
    /  * Address misaligned memory access is always allowed for ALL instructions.
    /  * Byte order on the memory is little-endian.
    /
    /  If it is the case, _WORD_ACCESS can also be set to 1 to improve performance and
    /  reduce code size. Following table shows an example of some processor types.
    /
    /   ARM7TDMI    0           ColdFire    0           V850E       0
    /   Cortex-M3   0           Z80         0/1         V850ES      0/1
    /   Cortex-M0   0           RX600(LE)   0/1         TLCS-870    0/1
    /   AVR         0/1         RX600(BE)   0           TLCS-900    0/1
    /   AVR32       0           RL78        0           R32C        0
    /   PIC18       0/1         SH-2        0           M16C        0/1
    /   PIC24       0           H8S         0           MSP430      0
    /   PIC32       0           H8/300H     0           x86         0/1
    */
    
    
    #endif /* _FFCONF */
    

    Jim

  • Hello Again:

    I have included ffconf.h and rebuilt the entire workspace (boot, drivers, platform, etc.).  The Boot Loader seizes up after displaying the initial message 'StarterWare AM335x Boot Loader' and before the 'Jumping to StarterWare Application...' message is displayed.  I suspect that it is getting stalled in the call to 'ImageCopy()' from bl-main.c. 

    Previously I was working with Starterware 02.00.01.01 with the BBB patches.  I had the sample project usb_host_msc working flawlessly.

    Can you offer any tips to troubleshoot my situation? 

    Respectfully,

    David

  • Hm, sorry, no, I don't have such problems here.

    I only noticed some troubles when configuring FatFS to use long filenames, then my application dies during boot (but amazingly _before_ any file system functions are called what lets me think about a compiler/linker/optimiser problem).

  • Hello Again:

    You may be onto something when you say it might be in the toolchain. Using the wildly inefficient (but effective) printf() debugging, I determinied that I am going off the rails inside the disk_initialize() function in fat_mmcsd.c. Specifically, the line " status = MMCSDCardInit(card->ctrl);".  The odd thing is that execution never makes it into MMCSDCardInit(). It seems to die in the function call itself.

    I will have another run at this ensuring that all of the optimizations are OFF.  I don't think I messed with those settings, but it might be worth a check.

    As another data point what  tools are you using? I am using CCSv5.5.0.00077 and TI Compilier 5.1.1.

    Respectfully,
    David      

  • > The odd thing is that execution never makes it into MMCSDCardInit()

    May be there is some pointer not inistialised before this call? As far as I remember there have been some file system related ones which need to be valid, but I'm not sure where they have been exactly...