The DM6433 datasheet shows that the Transition time, MXI/CLKIN is 0.05C(max). In the case of 27MHz clock, C = 37.037nS and the transition time is 1.85nS(max). This transition time seems to be very severe. Is there a crystal controlled oscillator which satisfies the transition specification and reasonable cost ? Also, DM6437EVM uses the oscillator ASFL3-27.000MHz-EK-T which transition specification (tr/tf) is 10nS. We do not understand how the ASFL3-27.000MHz-EK-T was selected and can be used on the DM6437EVM. So, please advice what specification of crystal oscillator can we select and use?
Best regards, Kazuaki Ohshita