HI,
I am trying to download a simple Hello word code to flash (Say nor flash) in CCS v 5, currently it is downloading into DDR2 of my EVM.
I am using Spectrum Digital davinci Evaluation module with JTAG Emulator.
I want to store the code even the power is off.
below is my linker command file:
-stack 0x00000800 /* Stack Size */
-heap 0x00000800 /* Heap Size */
MEMORY
{
IRAM: o = 0x00000000 l = 0x00004000
DRAM: o = 0x00008000 l = 0x00004000
AEMIF: o = 0x02000000 l = 0x02000000
DDR2: o = 0x80000000 l = 0x10000000
}
SECTIONS
{
.bss > DDR2
.cinit > DDR2
.cio > DDR2
.const > DDR2
.stack > DDR2
.sysmem > DDR2
.text > DDR2
.ddr2 > DDR2
}
Update:
Hi, I have gone through http://processors.wiki.ti.com/index.php/Serial_Boot_and_Flash_Loading_Utility , but a bit confused? It says downloading u boot, I want to flash (Download) my own application code say a hello word program to NAND/NOR.
I have generated a bin file of my program and want to download it to NOR flash and run the same when I power ON the EVM, please help me
I have been routed here from:
Regards,
Azhagiri S