This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem with Directfb on Davinci DM365



Hi all,

I have successfully cross compiled Directfb-1.2.0 for ti davinci DM365.

when i run the example code of directfb on the target it is running without any error,but i am not able to see any output on the tv display which is been connected with EVM.

I am not sure Directfb uses which window --- OSD or video window --- by default ?

Is their any configuration i need to make for either of these window, to get the directfb output to be seen on the tv display?

If yes then which are those configuration and how to do them?

 

Thanks....