Hi,
I work on the communication between two DSPs ( EP and RC ). I have two questions and I would like to have their answer :
Question 1 : When I debug my programs for the first time, the memory write transaction for example is done with success. Now , when I re debug for a second time the program, the transfer does not pass !!
I must turn OFF the two target ( EP and RC ), and again turn ON , after that , the transfer pass successful.
I think the PCIe module trun OFF automatically when i debug the program for a second time !! it's true?
Question 2 : my second question is about the MSI :
Suppose in our test, the EP sends an interrupt to the RC.
So the EP can know that the interruption has not been received in the RC side ?
can you give me an explanation of this questions please ?!
thank you,
Sincerely,
Zakaria.