Other Parts Discussed in Thread: OMAP3530
Hi all,
I'm trying to run the omap-demo on beagleboard, but the modules cmemk.ko, lpm_omap3530.ko, dsplinkk.ko and sdmak.ko are unable to be inserted.
When the loadmodules.sh script is invoked the following error-messages appear:
cmemk: disagrees about version of symbol find_vma
cmemk: Unknown symbol find_vma
cmemk: disagrees about version of symbol __register_chrdev
cmemk: Unknown symbol __register_chrdev
insmod: error inserting 'cmemk.ko': -1 Unknown symbol in module
dsplinkk: disagrees about version of symbol set_user_nice
dsplinkk: Unknown symbol set_user_nice
dsplinkk: disagrees about version of symbol wake_up_process
dsplinkk: Unknown symbol wake_up_process
dsplinkk: disagrees about version of symbol filp_close
dsplinkk: Unknown symbol filp_close
dsplinkk: disagrees about version of symbol __register_chrdev
dsplinkk: Unknown symbol __register_chrdev
insmod: error inserting 'dsplinkk.ko': -1 Unknown symbol in module
BusyBox v1.13.2 (2009-12-02 19:10:22 EST) multi-call binary
Usage: mknod [OPTIONS] NAME TYPE MAJOR MINOR
Create a special file (block, character, or pipe)
Options:
-m Create the special file using the specified mode (default a=rw)
TYPEs include:
b: Make a block device
c or u: Make a character device
p: Make a named pipe (MAJOR and MINOR are ignored)
lpm_omap3530: Unknown symbol IPS_notify
lpm_omap3530: Unknown symbol IPS_register
lpm_omap3530: Unknown symbol IPS_unregister
lpm_omap3530: disagrees about version of symbol cdev_add
lpm_omap3530: Unknown symbol cdev_add
lpm_omap3530: Unknown symbol LDRV_PROC_setState
lpm_omap3530: Unknown symbol LDRV_PROC_getState
lpm_omap3530: Unknown symbol PMGR_PROC_getSymbolAddress
lpm_omap3530: disagrees about version of symbol cdev_init
lpm_omap3530: Unknown symbol cdev_init
lpm_omap3530: disagrees about version of symbol cdev_del
lpm_omap3530: Unknown symbol cdev_del
insmod: error inserting 'lpm_omap3530.ko': -1 Unknown symbol in module
sdmak: disagrees about version of symbol put_page
sdmak: Unknown symbol put_page
sdmak: disagrees about version of symbol __register_chrdev
sdmak: Unknown symbol __register_chrdev
insmod: error inserting 'sdmak.ko': -1 Unknown symbol in module
root@omap3evm:/opt/dvsdk/omap3530# Demo interface started at level 0.
CMEM Error: init: Failed to open /dev/cmem: 'No such file or directory'
Error: Failed to create display device instance
sh: can't create /sys/devices/platform/omapdss/overlay0/global_alpha: nonexistent directory
Error: Failed to execute: echo 0 > /sys/devices/platform/omapdss/overlay0/global_alpha
I'm using dvsdk-3.01.00.03 + am35x-omap35x-psp-sdk-03.00.00.03 / linux.-2.6.32-rc5.
Any ideas will be of use.
Thanks in advance.